|
|
News - 2008
|
| |
|
|
 |
Precision version 2-Finger Parallel Gripper PGN-plus
|
|
 |
26.08.2008 -
The new precision versions of the proven and powerful PGN-plus series set new standards. A special modification has improved the minimal play and multi-tooth guided base jaws of the already high-precision gripper modules in terms of its clamping center, the gripper height and accurate
positioning when changing the gripper.
The advantages of the 2-finger parallel grippers which are even in height now, especially concern applications where several grippers are mounted on a mounting surface. This always ensures absolute parallelism of the gripper mounting surface to the mounting surface of the top jaws.
Even if a universal gripper is exchanged during maintenance works or set-up processes, an accurate positioning can be fully guaranteed. There is no need for re-teaching the controller program when the gripper module is re-installed.
|
|
| |
|
| |
|
|