|
|
News - Clamping Technology - Archive 2010
|
| |
02.09.2010
Hydraulic Expansion Toolholders - Most powerful than ever
With the TENDO E compact SCHUNK starts a new era in tool clamping. For the first time ever hydraulic expansion toolholders are available, which transfer torques of up to 900 Nm (at a 20 mm clamping diameter) safely and are absolutely adequate for volume cutting. With its excellent vibration damping and a very precise true-running accuracy of less than 0.003 mm at 2,5 x D, the precision mounting prevents the spindle but also the cutting edge from damage.
more...
30.08.2010
Magnetic Lifting Technology
Program for Lifting Magnets has been enlarged
SCHUNK, the competence leader in clamping technology and gripping systems is well-known for the MAGNOS magnetic clamping solutions. Just in time for the AMB show, SCHUNK presents their enlarged program for permanent lifting magnets, which can be manually and electrically actuated, and for the first time ever, pneumatically.
more...
09.08.2010
VERO-S: Quick-Change Pallet System of the next Generation
At the AMB Show in Stuttgart Germany, SCHUNK will showcase the quick-change pallet system for the next generation. The new set-up time killer is called VERO-S and will replace the SCHUNK UNILOCK module
more...
10.06.2010
Innovative Extensions are setting the Benchmark in Quality, Ergonomics, Set-up time and Cost
Operators, who have to precisely machine the deepest angle in the fields of tool and mold making, can breathe a sigh of relief! At the EMO show in Milan, Italy, SCHUNK GmbH, the specialist in toolholding, workholding and automation presented a long, slim hydraulic tool extension which works without any peripheral equipment and independent of the type of spindle interface. The extension converts almost any precision toolholder into a highly flexible specialist for tight machine rooms. The precise run-out accuracy, the excellent vibration dampening and even an internal coolant supply assure excellent workpiece machining results and long tool life.
more...
25.05.2010
SCHUNK strengthens distribution in China
More than ever before, China is the main focus of German machine builders. Within the next few years, SCHUNK would like to increase growth in the People’s Republic, and in preparation for this desired growth, SCHUNK has realigned their activities of distribution.
more...
25.01.2010
SCHUNK Laser Technology
Laser Welding for a Wide Range of Parts
SCHUNK presented its highly flexible laser welding machine for the partially automated deposition welding and repair welding of challenging materials and complex component geometries for the first time at Euromold in Frankfurt. The precision machine allows both small components and components weighing several tons to be machined quickly and conveniently.
more...
|
 |
 |
 |
|
News - Clamping Technology - 2013
News - Clamping Technology - Archive 2012
News - Clamping Technology - Archive 2011
News - Clamping Technology - Archive 2010
News - Clamping Technology - Archive 2009
News - Clamping Technology - Archive 2008
News - Clamping Technology - Archive 2007
News - Clamping Technology - Archive 2006
News - Clamping Technology - Archive 2005
News - Clamping Technology - Archive 2004
News - Clamping Technology - Archive 2003
|