25.11.2011
Producing more efficient
For a number of years, everybody was talking about the energy efficiency issue. Increasing energy costs, a growing environmental awareness, and the political guidance were all triggers for many companies to highlight the energy consumption of machines and components in their communication with the public. Efficiency is much more than simple energy efficiency now, especially when considering the
time- and cost aspects in regards to efficiency. When all these factors have been considered in a holistic way, the full potentials for modern machining and production become visible. The modern clamping devices and gripping systems make it clear how complex the possibilities are.
Pour en savoir plus…
08.11.2011
The most flat pneumatic Quick-Change Pallet Module in the world
SCHUNK, the competence leader for clamping technology and gripping
systems continues to enlarge its program of VERO-S Quick-Change Pallet System they will present at the EMO 2011 show. With a height of 20 mm, the VERO-S NSE mini module from SCHUNK is the most flat pneumatic Quick-Change Pallet Module in the world. This provides ideal conditions for retrofitting existing machines, making full use of the engine room, and allows direct clamping of small workpieces.
Pour en savoir plus…
28.10.2011
SCHUNK GmbH & Co. KG - A Short Profile
"To offer more than the customer expects", this was the motto of Friedrich Schunk, when he opened his machine shop in a garage in Lauffen, Germany, right after the troubles of World War II. Today, SCHUNK is a German innovative family-owned company and a global player all in one.
Pour en savoir plus…
26.10.2011
Status display for magnetic chucks
Operators will now be able to see at a glance whether the MAGNOS magnetic chucks from SCHUNK are activated or not. For this purpose, all the new square pole chucks from the competence leader for clamping technology and gripping systems are equipped with a permanent display which informs the operator on the clamping status of the magnetic chuck.
Pour en savoir plus…
20.10.2011
New Catalog for hydraulic expansion solutions
Customer-specific hydraulic expansion solutions are an effective possibility for minimizing set-up times and lowering costs at maximum precision. For presenting the large potential of this precision technology, SCHUNK, the competence leader for clamping technology and gripping systems has issued a catalog specifically for special solutions in the hydraulic expansion technology.
Pour en savoir plus…
15.08.2011
BLUE SIGMA - in total more efficient
On September 19 to 24 the EMO in Hanover, Germany will open its doors.
With the premiere of more than 40 benchmark products, SCHUNK as the compentence leader for clamping technology and gripping systems, is setting standards at the world-wide leading show for metalworking.
Pour en savoir plus…
11.08.2011
More precise in deepest angles
SCHUNK, the competence leader for clamping technology and gripping systems, has continued to enlarge its program of slim hydraulic extensions to be presented at the 2012 EMO show. With a shank diameter of 6 mm, the TENDO SVL tools can be directly clamped without the use of intermediate sleeves, making them highly precise.
Pour en savoir plus…
05.08.2011
A new catalog "Toolholding Systems"
Just in time for the EMO show, SCHUNK, the competence leader for clamping technology and gripping systems, is issuing a new catalog on toolholding systems. Highlights include the powerful TENDO-E hydraulic expansion toolholder and the TRIBOS-Mini, the first precision toolholder for direct clamping of very small shank diameters used for micro cutting. The catalog will hold the complete total tooling program of the innovative family-owned company.
Pour en savoir plus…
25.07.2011
Powerhouse for 5-axis machining
The KONTEC KSX NC vise from SCHUNK is a powerful clamping system for simultaneous 5-axis machining. The compact, and easily accessible clamping system from the competence leader for clamping technology and gripping systems disposes of tool-free adjustable clamping forces between 4 and 40 kN, which are measured directly at the workpiece. This is a great deal of power for a safe hold, even for minimum clamping surfaces.
Pour en savoir plus…
29.04.2011
Powerhouses for precise serial production
SCHUNK, the competence leader in clamping technology and gripping systems has completely reworked its series of TANDEM clamping blocks. Now they are part of a unique standardized modular system for highly-efficient workpiece clamping.
Pour en savoir plus…
21.04.2011
Clamping rings without deformation
SCHUNK has enlarged its program for highly efficient workpiece clamping. For exact machining of thin-walled rings on rotary tables, cylindrical grinding machines and lathes, the competence leader in clamping technology and gripping systems now offers a vast program of standardized magnetic chucks with radial pole pitch.
Pour en savoir plus…
30.03.2011
Secure hold per vacuum
With PLANOS, the vacuum clamping system from SCHUNK, two-dimensional and planar undersides of workpieces can be clamped quickly, easily and process-reliably with a vacuum at the machine table. Normally plates are very difficult to be handled and clamped mechanically, but even thin plates can be fixed precisely and deformation-free with PLANOS.
Pour en savoir plus…
21.03.2011
Ingenious helper cleans the machine tool
Manually blowing out chips is now a thing of the past. SCHUNK, the competence leader in clamping technology and gripping systems has developed a cleaning unit, which fits into tool mountings with a 20 mm diameter and can be converted into every machine tool.
Pour en savoir plus…
11.03.2011
Innovative clamping devices for TRIBOS polygonal technology
The SVP Mini and SVP-RM from SCHUNK are both safe and cost-effective clamping devices. Due to the pre-adjusted pressure, TRIBOS polygonal toolholders can be instantly mounted with them. This saves time and energy, reduces set-up costs, and eliminates operating errors.
Pour en savoir plus…
09.03.2011
Flexible lathe chuck increases efficiency during turning
The 3-jaw power chuck type ROTA NCD from SCHUNK, the competence leader in clamping technology and gripping systems is an all-rounder for high-precision workpiece clamping on lathes. It is particularly well suited for users who machine several workpieces on one machine and can reduce set-up times and costs with the high-performance lathe chuck.
Pour en savoir plus…
16.02.2011
New Lathe Chuck Catalog offers advanced know-how to the users
The SCHUNK lathe chuck catalog is now available. The catalog provides 660 pages information on the complete workholding program of SCHUNK, the competence leader in clamping technology and gripping systems. From lathe chucks to steady rests, jaw boxes up to accessories, everything is listed.
Pour en savoir plus…
01.02.2011
More toolholders with a Capto interface
Precision toolholding systems from SCHUNK are now equipped with the original Sandvik Coromant Capto interface. As a licensed partner of Sandvik Coromant, the competence leader in clamping technology and gripping systems manufactures TENDO hydraulic expansion toolholders, and other standardized toolholding systems with the original interfaces C4, C5, C6 and C8.
Pour en savoir plus…
20.01.2011
TENDOzero: To 0.000 mm in no time
Micron precision is always required for drilling, reaming and line boring. Now SCHUNK, the competence leader in clamping technology and gripping systems, offers a hydraulic expansion toolholder, where a run-out accuracy of 0.000 mm can be quickly adjusted.
Pour en savoir plus…
|