14.05.2013
World Premiere: Standardized Long-Stroke Gripper with CFC Housing
The CGH long-stroke gripper from SCHUNK is a milestone in handling: For the first time SCHUNK, the competence leader for clamping technology and gripping systems succeeded in standardizing a light-weight gripper with CFC housings. The versatile module convinces in terms of energy-efficiency and economic efficiency. It helps to increase dynamics of existing systems, or enables the use of smaller robots.
más…
11.04.2013
La automatización y la cualificación crean puestos de trabajo
La charla técnica con el portero estrella organizada por SCHUNK, líder experto en técnica de sujeción y sistemas de agarre, que tuvo lugar el martes en la feria de Hannover contó con una gran afluencia de famosos. En este acto presentado por Jessica Kastrop, la cautivadora reportera jefe responsable de la Champions League de la cadena Sky, participaron Henrik A. Schunk, socio gerente de SCHUNK, el Dr. Till Reuter, director ejecutivo de KUKA, el Dr. Hubert Waltl, miembro de la directiva de Volkswagen, el Prof. Dr. Thomas Bauernhansl, director del Instituto de Producción Industrial y Sistemas Fabriles de Stuttgart y del Instituto Fraunhofer de Técnicas de Producción y Automatización, así como Jens Lehman, portero legendario, y trataron el tema "la automatización como factor de éxito".
más…
09.04.2013
Quick-change fingers increase flexibility of assembly systems
SCHUNK, the competence leader for clamping technology and gripping systems, has transferred its extensive experience with quick-change systems to the design of gripper fingers. The innovative family-owned company introduces a new type of finger blank with a quick-change system already integrated as a standard feature. The quick-change fingers allow users to minimize setup times when changing over to a new parts spectrum, resulting in increased productivity and flexibility of the overall system.
más…
04.04.2013
Service Robotics: A Vision becomes Reality
Dr. Roko Tschakarow, Business Director Mobile Gripping Systems at SCHUNK, speaks about the future and the challenges of service robotics.
más…
26.03.2013
Mobile gripping systems: catalog and website completely revised
The 6th Expert Days on Service Robotics have only just concluded and SCHUNK has already added a new touch to mobile gripping systems: a new catalog and the newly designed website provide an up-to-date overview of SCHUNK's wide ranging module selection for mobile applications in service robotics.
más…
22.03.2013
Precise partners for automated pallet change
SCHUNK, the competence leader for clamping technology and gripping systems has developed the VERO-S NSA plus palletizing module and the VERO-S NSR robot coupling for automated pallet change. Both are extremely flat, work precisely, and ensure consistently high process stability. With the fast and clamping strokes patented by SCHUNK, the palletizing module achieves pull-in forces of up to 20.000 N.
más…
22.03.2013
red dot Award for the Powerball Arm from SCHUNK
SCHUNK, the competence leader for clamping technology and gripping systems has reason to celebrate: The Powerball Lightweight Arm LWA 4P wins the red dot Award: Product Design 2013. The exclusive principle of design behind the powerful lightweight arm convinced the jury of 37 experts of the internationally renowned competition even though the field of applicants was very large: This year the number of submissions amounted to 4,662 submissions in 19 different categories.
más…
06.03.2013
Rapid Pick & Place for loads up to 5 kg
The linear directly driven Pick & Place units of the PPU-E series from SCHUNK are considered to be the fastest pick & place units on the market. The largest size PPU-E 50, is an expert for dynamic handling of medium-weight masses up to 5 kg. For a complete cycle with a 280 mm horizontal and 150 mm vertical stroke the unit has a cycle time of 0.92 seconds with a tooling mass of 2 kg and 2 x 60 ms (for gripper).
más…
22.01.2013
Rapid Module for short strokes
Horizontal or vertical: if small, highly dynamic loads need to be moved over short distances, the linear directly driven SLD short stroke module from SCHUNK, the competence leader for clamping technology and gripping systems is up for the challenge. Compared with its predecessor module, the high-performance servo motor of the LDK is achieving a 15% higher nominal force.
más…
18.01.2013
Compact Rotary Module with pneumatic and electric Feed-Through
SCHUNK, the competence leader for clamping technology and gripping systems has enlarged its program of intelligent mechatronic modules. With the ERS DFF, the innovative family-owned company is setting a new benchmark for swivel units: It is the most compact electric rotary module with combined pneumatic and electric feed-through in the market. The module is based on the flat ERS rotary module, which is equipped with a torque motor with hollow shaft.
más…
11.06.2012
Desbarbado con robot
Hasta ahora, siempre ha sido difícil desbarbar con un robot, aquellos contornos de piezas que son complejos. Las rebabas, o bien no se eliminaban correctamente o bien se procedía a arrancar más material de lo deseado, provocando un desgaste rápido de la herramienta, hasta incluso la rotura. El FDB de SCHUNK, con su husillo de alta frecuencia protegido y patentado, corrige esos puntos débiles. Se obtiene más flexibilidad, usando herramientas adaptables, que compensen las desviaciones entre la trayectoria del robot y el contorno de la pieza. Como resultado, esto nos da un mejor acabado de la pieza, reduciendo los costes en herramientas y acortando los tiempos de programación y puesta en marcha.
más…
06.06.2012
Alta eficiencia en el manipulado de piezas pequeñas
SCHUNK comienza una nueva era en la manipulación de piezas pequeñas con su mini pinza paralela MPG-plus. Comparando con módulos similares que necesitan el mismo input, la nueva pinza de manipulado de piezas pequeñas de SCHUNK, consigue un output muy superior. Por este motivo, establece estándares hacia sistemas cada vez más pequeños y eficientes.
más…
06.06.2012
Pinzas de alta velocidad, para paneles solares.
La SZG-C de SCHUNK, es una pinza altamente dinámica para la manipulación de paneles solares. Esta pinza manipula de forma segura, precisa y con absoluta suavidad, los paneles y las células acabadas. Debido a su capacidad de dejar pieza con rapidez, esta pinza ligera puede llevar a cabo un ciclo de transporte completo de 550 mm, incluida una rápida inspección con un sistema de cámara y la vuelta a la posición inicial, en un tiempo de ciclo inferior a un segundo.
más…
06.06.2012
Sensor magnético universal programable
Controlar una pinza neumática durante las tareas de manipulación puede ser ahora mucho más fácil. El sensor magnético MMS 22-Pl1 de SCHUNK, utiliza los puntos de programación, convirtiéndolo en un sensor multifuncional. En vez de usar diversos sistemas, un único sensor puede ser suficiente. Los componentes que lo integran se han reducido en tamaño, para dotarle de una mayor flexibilidad. El control se lleva a cabo mediante un imán colocado en el interior del actuador. Desde el punto de programación se pueden ajustar las posiciones de forma individual. El actuador puede ser introducido en la ranura completamente sin necesidad de que ningún contorno perturbante interfiera.
más…
01.06.2012
Sistema de paletizado, todo en uno.
La pinza para paletizado LEG del experto en técnicas de sujeción SCHUNK, es una auténtica todo terreno: podrá manipular pallets, hacer cambios de forma flexible y colocar capas de distintos niveles para diversos productos. El corazón de este sistema multifunción, es la pinza paralela servo controlada LEG de SCHUNK. Estas pinzas se pueden integrar con una gran variedad de motores. De forma muy sencilla podrá mover el robot y la pinza sincronizadamente a través de una interfaz de usuario. La pinza tiene una exactitud de posicionado muy alta y trabaja de forma flexible con recorridos de hasta 281 mm de carrera por mordaza. Con la ayuda de un control de potencia, también podrá manejar productos de distinta fragilidad.
más…
|