|
|
Noticias - Técnica de fijación - 2013
|
| |
10.06.2013
Efficient extras for clamping force blocks
SCHUNK, the competence leader for clamping technology and gripping systems extends its series of TANDEM KSP plus clamping force blocks with two helpful extras. With the jaw quick-change system BWM clamping blocks can be retrofitted independent from its installation position in less than 30 seconds onto a new chuck jaw set for O.D. clamping.
más…
06.05.2013
Universal high-performance lathe chucks
The ROTA NCD wedge bar power chuck from SCHUNK is extremely versatile. It is used for clamping small diameters as quickly and precisely as large ones. Instead of exchanging lathe chucks and collet chucks, which can be tedious, just the top jaws of the ROTA NCD have to be exchanged against special collet jaws. This minimizes set-up times and allows a considerably higher output.
más…
02.05.2013
Special Program for Micro Cutting
No matter where toolholders are used: mold making, dental technology, medical technology, clock- and jewelry industry - the number of high-precision applications in the field of micro cutting has enormously increased in the past few years. Since conventional clamping systems most often reach their limits, SCHUNK, the competence leader of clamping technology and gripping system has enlarged its precision toolholder program for micro cutting. New interfaces and a higher degree of standardization will help the user increase process reliability and efficiency of demanding precision applications.
más…
18.04.2013
Greater efficiency with integrated vibration damping
Manufactures who produce precision turned parts in large quantities have to consider several factors. Tolerances and surface qualities have to be precisely maintained, set-up times, downtimes, and tool wear have to be reduced. The TENDOturn hydraulic expansion toolholders from SCHUNK make everything feasible. The set-up process of the latest toolholder generation of the competence leader in clamping technology and gripping systems has been further simplified.
más…
26.02.2013
Extremely flat pneumatic Quick-Change Pallet Module
With a height of 20 mm, the Quick-Change Pallet Module VERO-S NSE mini from SCHUNK is extremely flat. This provides ideal conditions for retrofitting existing machines, making full use of the engine room, and allows direct clamping of small workpieces. The patented drive concept consists of a fast stroke and a clamping stroke, and ensures that the compact module of the innovative family-owned company has a highly compact performance.
más…
21.01.2013
Versatile manual lathe chuck
The manual ROTA-S plus lathe chuck from SCHUNK is a true classic in the field of lathe chuck technology. With version 2.0, the competence leader for clamping technology and gripping systems extends the application possibilities of this lathe chuck. An optimized wedge bar drive system and an improved lubricant system ensure consistently high clamping forces from the new lathe chuck.
más…
17.01.2013
Direct clamping with a membrane
SCHUNK, the competence leader for clamping technology and gripping systems enlarges its program for high-performance direct clamping: the innovative family-owned company has developed the SPM plus 138 fixture membrane made of aluminum, where workpieces of various clamping geometries are clamped from all sides with a pull-down effect.
más…
10.01.2013
Low-cost introduction into the square pole technology
By means of comprehensive standardization, SCHUNK, the competence leader for clamping technology and gripping systems succeeded in providing a very economic introduction of the square pole technology to the average consumer. The investment costs for square pole plates of the MAGNOS Performance Line are 40% lower than conventional, multi-purpose modifiable MAGNOS square pole plates.
más…
11.06.2012
Técnica de elevación magnética
Ampliado el programa de electroimanes elevadores
Hace mucho tiempo que se conoce al fabricante especialista en técnicas de sujeción y agarre SCHUNK, por sus inteligentes soluciones en el ámbito de la fijación magnética, MAGNOS. SCHUNK ha ampliado considerablemente su programa en el sector de los electroimanes permanentes y elevadores. A parte de los módulos elevadores con accionamiento manual o eléctrico, como novedad se ofrecen módulos de accionamiento neumático. Con esta solución, SCHUNK acerca la conocida tecnología magnética hacia los manipuladores, balanceadores y las soluciones de automación y robótica. Los módulos son fácilmente actuados con aire comprimido, lo que reduce considerablemente la puesta en marcha.
más…
11.06.2012
Mordazas compactas: máxima energía, para una producción de precisión en serie.
El experto en técnicas de agarre y sistemas de sujeción SCHUNK, ha revisado por completo sus bloques de sujeción compactos. Por lo que ya forman parte del único y estandarizado sistema de construcción para amarrar piezas a mecanizar de forma eficiente. Los bloques de sujeción compactos proporcionan a la misma vez fuerza y precisión. Son de diseño extremadamente compacto y desarrollan una enorme fuerza en espacios reducidos, por lo que la máquina herramienta se optimiza. Opcionalmente, pueden ser accionados por neumática, hidráulica, por muelle o de forma manual.
más…
06.06.2012
El módulo neumático a punto cero más plano del mundo
SCHUNK, experto en técnicas de sujeción y sistemas de agarre, amplia su programa VERO-S, sistema de cambio rápido de pallets. Con una altura de 20 mm, el módulo VERO-S NSE mini de SCHUNK, es el módulo neumático a punto cero más plano del mundo. Condición ideal para el retrofitting de máquinas existentes y el aprovechamiento al máximo del espacio de la máquina. Además permite la fijación directa de piezas pequeñas.
más…
|
 |
 |
 |
|
Noticias - Técnica de fijación - 2013
Noticias - Técnica de fijación - Archivo 2012
Noticias - Técnica de fijación - Archivo 2011
Noticias - Técnica de fijación - Archivo 2010
Noticias - Técnica de fijación - Archivo 2009
Noticias - Técnica de fijación - Archivo 2008
Noticias - Técnica de fijación - Archivo 2007
Noticias - Técnica de fijación - Archivo 2006
Noticias - Técnica de fijación - Archivo 2005
Noticias - Técnica de fijación - Archivo 2004
|