|
SCHUNK vu par la presse - Archives 2009
|
| |
|
CIM - Canadian Industrial Machinery, Août 2009
Distorting - The Facts
The fact that workholding distorts workpieces is a common challenge facing manufacturers. The forces applied while holding the part invariably alter its shape, and when it’s released from the holding device, it typically springs back to its original condition.
|
Pour en savoir plus… |
|
Lathe Chucks
|
|
|
Machinery Market, Juin 2009
Tool extension makes life much easier
The TENDO extension module from Schunk Intec Ltd., Newport Pagnell, has been developed to make life easier for tool makers and die makers. This long, slim hydraulic-expansion extension dispenses with the need for auxiliary equipment and can transform any precision holder into a versatile tool for narrow spaces, independent of the spindle interface.
|
Pour en savoir plus… |
|
TENDOturn
|
|
|
Drives & Controls, Mai 2009
Add-on valve cuts assembly costs
Schunk has launched a series of miniature pneumatic valves that can be screwed directly into actuators, cutting the cost of hosing between the valve and the actuator. The hose-free assembly reduces wiring for power supplies and signalling, and is said to save compressed air because the supply line does not need to be filled and emptied on each cycle.
|
Pour en savoir plus… |
|
|
|
|
Engineering Subcontractor, Mai 2009
Hydraulic clamping steers clear of rejection
The hydraulically clamped precision tool holders from the TENDO range from Lauffen-based clamping and gripping specialist SCHUNK ensure maximum vibration damping. The user benefits from brilliant surfaces and from considerably prolonged service life of tools used.
|
Pour en savoir plus… |
|
TENDOturn
|
|
|
Machinery World, Mai 2009
ABV add-on valve reduces assembly costs
Schunk has launched a series of miniaturized MV-series pneumatic valves that can be screwed directly into the corresponding actuator to reduce the cost for hosing between the valve and the actuator. This hose-free assembly of the micro valves to the actuators also saves valuable compressed air, as each cycle no longer requires the entire supply line to b filled and emptied, which reduces the cycle times.
|
Pour en savoir plus… |
|
|
|
|
Production Engineering Solutions, Mai 2009
Precision all round
An all rounder for the high precision clamping of workpieces on a lathe is the 3-jaw power chuck ROTA NCD from Schunk Intec. According to Schunk, users processing different workpieces on a sungle machine can now significantly reduce set-up times and costs.
|
Pour en savoir plus… |
|
ROTA NCD
|
|
|
Engineering Subcontractor, Avril 2009
Long extension is a lifeline in deep cavities
Innovative module sets standards. Those in the tool and die industry having to carry out precision work in even the deepest of cavities can breathe a sigh of relief. At a recent exhibition, the Lauffen-based toolholding and workholding specialist Schunk Intec presented a long, slim hydraulic expansion extension that dispenses with the need for auxiliary equipment and can transform almost any precision toolholder into a versatile tool for narrow spaces independent of the spindle interface.
|
Pour en savoir plus… |
|
ROTA NCD
|
|
|
Industrial Technology, Avril 2009
Centric grippers with multitooth guidance
The PZB-plus from Schunk Intec is a newly designed series of 3-finger centric grippers with a special feature that is a central bore designed as fitting. This central bore feature is equipped with female threads for customer-specific add-ons and can be used to supply material or as an ejector.
|
Pour en savoir plus… |
|
Universal gripper PZB-plus
|
|
|
Machinery World, Avril 2009
Like an elephant walking a tightrope
At SHW Bearbeitungstechnik GmbH in Aalen-Wasseralfingen, Germany, extremes of size come together with workpieces weighing serveral tons on the one hand and precision machining in the micron range on the other.
|
Pour en savoir plus… |
|
TRIBOS-R
|
|
|
Engineering Subcontractor, Mars 2009
An investment that will forever hold your piece
At SHW Bearbeitungstechnik GmbH in Aalen-Wasseralfingen, Germany, extremes of size come together with workpieces weighing several tons on the one hand and precision machining in the micronrange on the other.
|
Pour en savoir plus… |
|
MAGNOS Magnetic Clamping Technology
TRIBOS-R
|
|
|
MTI, Janvier 2009
SCHUNK expert forum
The German clamping and gripping specialist SCHUNK GmbH will be holding 'Service Robotics Expert Days' on 18-19 February at Brackenheim-Hausen in Germany.
|
Pour en savoir plus… |
|
SCHUNK ExpertDays
|
| |
| |
SCHUNK vu par la presse - Archives 2012
SCHUNK vu par la presse - Archives 2011
SCHUNK vu par la presse - Archives 2009
SCHUNK vu par la presse - Archives 2008
SCHUNK vu par la presse - Archives 2007
SCHUNK vu par la presse - Archives 2006
SCHUNK vu par la presse - Archives 2005
SCHUNK vu par la presse - Archives 2004
SCHUNK vu par la presse - Archives 2003
SCHUNK vu par la presse - Archives 2002
SCHUNK vu par la presse - Archives 2001
|
|
|