|
|
Press Release - Clamping Technology - Archive 2006
|
| |
|
14.09.2006
KONTEC KSC - the all-rounder
KONTEC KSC is the centric-clamping device and single-acting vise for nearly all workpieces, irrespective of whether conventional clamping is involved, whether very small clamping depths for five-sided machining are required, or whether molded parts, plates or workpieces with saw cuts are concerned - KONTEC KSC ensures that adjustments can be made in no time at all.
more...
|
|
|
14.09.2006
KONTEC KSS - the mechanical clamping force powerhouse
What previously only seemed possible either pneumatically or hydraulically can now be achieved very simply and with a single hand movement with the KONTEC KSS - 10% to 100% of the clamping force with just one crank rotation! Always with the same crank end position.
KONTEC KSS also guarantees the highest possible level of safety when machining, as a mechanical lock secures the preset clamping force and ensures an extremely high degree of repeat accuracy.
more...
|
|
|
14.09.2006
Presetting device with integrated TRIBOS clamping system
Those who are already working with the TRIBOS precision clamping device in their production facility shouldn’t have to do without the new SCHUNK presetting device any longer. Because, when used with the TRIBOS Polygonal Clamping Technology, this highly-accurate, optical tool presetting and measuring device, in conjunction with the TRIBOS precision clamping equipment, raises every quality standard by a significant amount.
more...
|
|
|
20.06.2006
MAGNOS MLH lifting magnets – faster and safer workpiece transportation
MAGNOS MLH lifting magnets have been incorporated into the SCHUNK product range as an addition to the MAGNOS magnetic clamping technology. By using these lifting magnets you will reduce your workpiece transportation times as well as significantly increase the safety of workpiece transportation.
The lifting magnets are available in five different sizes and have a maximum lifting power of 2,000 kg.
more...
|
|
|
20.06.2006
New – UNILOCK quick change pallet module NSE 138-T - the "set-up time killer"
Locate, position and clamp workpieces and devices in one single operation.
This means reducing set-up times to a minimum!
A new addition to SCHUNK’s product range of quick change pallet systems is the NSE 138-T.
The new NSE 138-T assembly module was especially designed for tombstones. Thanks to its minimal mounting height of 11 mm, it can be positioned and mounted directly on the plane surface of tombstones.
more...
|
|
|
20.06.2006
Wireless RSS pressure monitoring for optimum production reliability
For monitoring clamping pressure with lathe chuck for O.D. clamping operations. By means of wireless sensor systems, the clamping pressure is monitored automatically and regularly, even during machining. The signal is transmitted directly to the machine control system via the transmitter unit.
more...
|
|
|
20.06.2006
New GZB-S intermediate sleeves for TENDO hydraulic expansion toolholder for extremely small clamping diameters starting from 0.8 mm
The new TENDO GZB-S intermediate sleeves (outside diameter – 8 mm) supplement the range of existing intermediate sleeves. The clamping range extends from 0.8 to 6.0 mm, in increments of 0.1 millimeters.
more...
|
|
|
09.01.2006
Universal Top Jaws
Universal top jaws from Lauffen’s SCHUNK GmbH & Co. KG with metric tongue and groove can be used in all wedge-bar power chucks (with quick jaw change). The flexibility of these jaws reduces set-up times and costs, especially for small and variable batch sizes.
more...
|
|
|
09.01.2006
ROTA NCR precision 6-jaw power chucks
More precision – even for the most difficult applications.
more...
|
|
|
09.01.2006
KONTEC KSL-VS
Production without waste
Unique clamping system with quick jaw adjustment - now also available with enlarged clamping width
more...
|
|
|
09.01.2006
TENDOturn hydraulic expansion technology for lathes
With the addition of TENDOturn, SCHUNK is enlarging its product range in the area of hydraulic expansion technology for lathes. With most lathe applications, vibrations are the greatest challenge. Vibrations can have adverse effects on tool life and the surface quality of workpieces. Thanks to systems from the TENDOturn series, vibration dampening has been increased significantly.
more...
|
|
|
03.01.2006
ROTA NCF plus precision power chucks
SCHUNK’s new ROTA NCF plus power chuck has been developed to meet the high requirements of modern lathes.
more...
|
|
|
03.01.2006
SINO universal toolholders
With the consistent TOTAL TOOLING strategy, SCHUNK has set global standards in the field of toolholding. The comprehensive range is based on expertise and precision, the products’ success on innovation and continuity.
more...
|
|
|
03.01.2006
MAGNOS magnetic clamping system
As a permanent magnet or an electropermanent magnet, for rough or fine cutting, SCHUNK offers the ideal solution.
more...
|
|
|
Press Release - Clamping Technology - 2013
Press Release - Clamping Technology - Archive 2012
Press Release - Clamping Technology - Archive 2011
Press Release - Clamping Technology - Archive 2010
Press Release - Clamping Technology - Archive 2009
Press Release - Clamping Technology - Archive 2008
Press Release - Clamping Technology - Archive 2007
Press Release - Clamping Technology - Archive 2006
Press Release - Clamping Technology - Archive 2005
Press Release - Clamping Technology - Archive 2004
Press Release - Clamping Technology - Archive 2003
|
|
|