|
|
Communiqués de presse - Modules de Préhension - Archives 2010
|
| |
|
15.12.2010
iF Design Award for Modular Long-Stroke Grippers
The PHL from SCHUNK outperformes in efficiency and design
The newly developed PHL long-stroke gripper from SCHUNK combines in a unique manner, technological know-how and functional, appealing design. As one of the first long-stroke gripper ever, it optionally disposes of a multi-tooth guidance or a profiled rail guidance, which considerably increases the module’s degree of efficiency. For this successful symbiosis, the gripper was recently awarded with the iF Product Design Award 2011.
Pour en savoir plus…
|
|
|
15.11.2010
Teaching Grippers to see
SCHUNK, the competence leader in clamping technology and gripping systems has enlarged its vast modular system of grippers again. As the first ever standardized gripper, the PGN-plus universal gripper, and the MPG-plus gripper for small components from SCHUNK are now equipped with an integrated distance and presence sensor. With the new OAS, both modules quickly transform into seeing grippers without needing an expensive vision system.
Pour en savoir plus…
|
|
|
15.11.2010
LEG 400 - Modular lightweight gripper with long stroke
SCHUNK is continuing to extend its range of modular long-stroke electric grippers: with the LEG 400 gripper, users involved in the cutting of metal products, the automotive industry as well as assembly and handling tasks are now also able to make use of the benefits of modular gripping. The weight-reduced lightweight gripper is equipped with a servo motor and has a gripping force of up to 1050 N as well as a variable stroke between zero and 103 mm. With one motor, it weighs only 6.5 kg.
Pour en savoir plus…
|
|
|
15.11.2010
SWS-I
Robotic Tool Change System with integrated valves
By using micro valves, handling processes can be created more efficiently. At the quick-change systems used for robots, cycle times can be reduced, and air consumption of the attached actuators is lowered. Now SCHUNK offers a vast program of highly efficient valve adapter plates for quick-change systems, which opens up potential for enhanced efficiency.
Pour en savoir plus…
|
|
|
10.11.2010
SCHUNK Expert Days Service Robotics 2011
Symposium illuminates the Market Potentials of
Service Robotics
Research, development trends, and efficiency will be the main topics on the agenda at the SCHUNK Expert Days Service Robotics 2011. From February 23 and February 24, 2011, SCHUNK the competence leader for clamping technology and gripping systems, will meet experts in service robotics from all over the world. The international symposium of the commited family-owned company will take place in 2011 for the fourth year in succession at the SCHUNK automation plant in Brackenheim-Hausen. It is considered to be the worldwide leading communication platform for applied service robotics.
Pour en savoir plus…
|
|
|
05.10.2010
Ingenious helper cleans the machine tool
Manually blowing out chips is now a thing of the past. SCHUNK, the competence leader in clamping technology and gripping systems has developed a cleaning unit, which fits into tool mountings with a 20 mm diameter and can be converted into every machine tool. A small control program quickly cleans the working area, tables, and clamping devices from chips. The machine carries out this job faster and more systematically than any operator could.
Pour en savoir plus…
|
|
|
05.10.2010
TENDOzero: To 0.000 mm in no time
Micron precision is always required for drilling, reaming and line boring. Now SCHUNK, the competence leader in clamping technology and gripping systems, offers a hydraulic expansion toolholder, where a run-out accuracy of 0.000 mm can be quickly adjusted. The TENDOzero is equipped with four lateral set-screws, which directly affect the tool shank, the angular position of the tool is corrected, and run-out is precisely adjusted. With this precision toolholder from an innovative family-owned company, even demanding applications with tight tolerances of shape, position and surface quality are carried out quickly and reliably.
Pour en savoir plus…
|
|
|
13.09.2010
PZH-plus: Powerhouse with long Stroke
When components of different sizes have to be handled alternately, conventional centric grippers quickly reach their limits. In order to cover the whole spectrum of components, gripper fingers or complete grippers have to be exchanged over and over again. The competence leader in clamping technology and gripping systems, SCHUNK, offers a highly efficient alternative: the innovative Long Stroke Gripper PZH-plus. The belt drive disposes of a long stroke, and the exchange of top jaws or grippers are now obsolete.
Pour en savoir plus…
|
|
|
13.09.2010
Compact Valve Boxes are the pace-makers
Seamlessly integrated micro valves have the best potential for achieving high performance in handling. For direct attachment to the PGN-plus universal gripper, SCHUNK now offers a compact valve box, which helps to increase actuation speed by up to 100 percent. At higher cycle rates, a reduction of the cycle time by 20 ms for 3 months saves a complete shift. At the same time, the valve box reduces the compressed air consumption and in turn reduces energy costs. Even existing handling systems can be easily retrofitted with the module.
Pour en savoir plus…
|
|
|
13.09.2010
Angular and Parallel Gripper in one Unit
The angular parallel gripper GAP from SCHUNK combines the advantages of two principles of gripping. Depending on the design, the gripper disposes of an opening angle between 30° and 180°. The parallel movement assures maximum precision and a high gripping force between 80 and 340 N on the last few millimeters. Workpieces with an overhang or interfering contours can be gripped without problems. In contrast to conventional angular grippers, the gripping center is always maintained, and even parts with various diameters can be handled and centered precisely.
Pour en savoir plus…
|
|
|
13.09.2010
Precise Stroke Module
The new HLM Stroke Module from SCHUNK is compact, precise and resilient. The rigid design and the hydraulic dampening of the end positions allow minimum cycle times. Therefore the module from the competence leader in clamping technology and gripping systems is ideal for automated high-performance assembly. Due to the compact design, and the high compact performance, it can be also used highly efficient in narrow installation spaces. Pre-clamped, scope-free cross roller guidances assure a high guiding accuracy and precision. At a repeat accuracy of 0.01 mm, even very precise applications can be carried out process reliably.
Pour en savoir plus…
|
|
|
13.09.2010
High tech from nature
Innovative materials will always play an important role for future gripping systems. "The lightweight design offers a high potential of efficiency enhancement," emphazises Matthias Poguntke, Head of Product Management of the Business Unit Automation at SCHUNK. "Lightweight solutions save energy at the same performance or achieve an even higher performance at the same energy consumption. In both cases the efficiency of the overall system profits from it." According to Mr. Poguntke, "This is the reason why the lightweight designs are so interesting for plant manufacturers, system integrators and also for operators.
Pour en savoir plus…
|
|
|
06.08.2010
Controlling grippers with an iPad
With WSG 50, SCHUNK, the competence leader in clamping technology and gripping systems is now able to offer a sensitive gripper for the first time that can be controlled via Ethernet TCP/IP in addition to Profibus DP and that also has an integrated Web server for configuration and diagnostics. That makes programming, putting it into operation, remote maintenance and its provision with updates with an Apple iPad for example, extremely simple. The two communication protocols and
the integrated control and regulation electronics ensure maximum flexibility when integrated into higher-order systems. The gripper of the innovative family-owned company is equipped with an internal MicroSD card for saving programs and documents.
Pour en savoir plus…
|
|
|
27.07.2010
Program for Lifting Magnets has been enlarged
SCHUNK, the competence leader in clamping technology and gripping systems is well-known for the MAGNOS magnetic clamping solutions. Just in time for the AMB show, SCHUNK presents their enlarged program for permanent lifting magnets, which can be manually and electrically actuated, and for the first time ever, pneumatically. By offering this option, SCHUNK transfers the proven magnetic technology onto pneumatically actuated manipulators, balancers and automated solutions. Since the modules are easily actuated with compressed air, costs for commissioning are drastically reduced.
Pour en savoir plus…
|
|
|
24.06.2010
Linear module D 90: Small and quiet
SCHUNK has enlarged the series of compact linear modules from the HSB system for miniaturization.
Pour en savoir plus…
|
|
|
10.06.2010
SCHUNK’s MPG-plus received the MM Award
With the MPG-plus Miniature Parallel Gripper, SCHUNK brings about new solutions for the handling of small components. Compared with similar modules which require the same input, the new SCHUNK gripper for small components achieves a considerably higher output, clearing the way for smaller and more efficient systems. At the Automatica show 2010, this power gripper received the MM Award in the category "gripping technology" of the renowned magazine MM MaschinenMarkt.
Pour en savoir plus…
|
|
|
08.06.2010
Robotic Tool Change System with integrated piston stroke control
The program of standardized robotic tool change systems with integrated piston stroke monitoring from SCHUNK has been enlarged. With the improved SWS-040 and the completely new SWS-076 SCHUNK now offers seven sizes with integrated monitoring. It helps to monitor the condition of the tool change system, to minimize the unit’s size, and to increase process reliability.
Pour en savoir plus…
|
|
|
08.06.2010
Powerball makes service robots mobile
The automation specialist SCHUNK from Lauffen in Germany has further expanded its modular robotics range with the SPB Powerball. For the first time, the movements of two axes are combined in a single module in extremely compact space. The powerful module provides high torques. It can be used to implement compact lightweight arms, service robots and other handling applications with a modular structure.
Pour en savoir plus…
|
|
|
08.06.2010
Up to 95 Picks per Minute
The pneumatically driven PPU-P unit from SCHUNK makes rapid Pick & Place possible. With up to 95 cycles per minute, it is the fastest pneumatic Pick & Place Unit on the market. Thanks to the control unit, the gripper can be placed directly over the individual target position, and is actuated through the standard control interface.
Pour en savoir plus…
|
|
|
08.06.2010
Modular Long Stroke Gripper: The new Power Generation
With the PHL, SCHUNK launches a new generation of long stroke grippers. The PHL from SCHUNK alternatively disposes of a multi-tooth guidance or a profiled rail guidance, which increases the degree of efficiency of the module. More importantly, the modular design of the PHL offers 90 standardized versions from the beginning! Thus over-sizing is avoided, the consumption of compressed air and energy is minimized, and the required space for applications is reduced. With the PHL, SCHUNK makes efficient gripping of large strokes possible.
Pour en savoir plus…
|
|
|
08.06.2010
Very efficient handling of small components
With the MPG-plus Miniature Parallel Gripper, SCHUNK brings about new solutions for the handling of small components. Compared with similar modules which require the same input, the new SCHUNK gripper for small components achieves a considerably higher output, clearing the way for smaller and more efficient systems.
Pour en savoir plus…
|
|
|
08.06.2010
Very efficient lightweight axis made of carbon fiber
Components made of carbon fiber are making many advances in racing and automotive engineering. With the CFK-axis system CLD, SCHUNK is now showcasing for the first time, a standardized linear axis made of carbon fiber. It is the lightest directly driven linear axis on the market. Compared with aluminum profiles, the weight of the profile reduces by 58 per cent. For multi-axis handling systems, where complete Z- or Y axis are moved, the lightweight design ensures efficiency and helps the axes to accelerate, saving a lot of energy in the process.
Pour en savoir plus…
|
|
|
25.05.2010
Efficient grippers for hygienic pharmaceutical production
SCHUNK has developed a gripping system particularly with the requirements of the pharmaceutical industry and laboratory automation in mind. SCG Sterigrip fulfilles all the requirements for cleanroom class 1 applications. This hygienic gripper is made of stainless steel weighing 160 grams. With a unique patented drive concept, the angular gripper defines a completely new dimension of performance amongst pneumatic grippers.
Pour en savoir plus…
|
|
|
19.04.2010
Adjustable Compensation Units without pneumatic system
Even if deviations in position and tolerances of robot and workpieces have to be compensated, SCHUNK offers a vast product portofolio of compensation units, which help the robot avoid malfunctions and damages to the tooling or part and assures more efficiency and process reliability. At the Automatica 2010 SCHUNK showcase three compensation units, which operate without a pneumatic system.
Pour en savoir plus…
|
|
|
12.04.2010
Efficient, flexible and affordable
Components used for service robotics have to be light-weight, but also have to quickly move relatively heavy loads. The industry-prooven LWA 3 light-weight arm from SCHUNK combines both aspects. Its light, rigid design and its efficient drives currently makes it the most efficient modular light-weight arm on the international market. It disposes of a weight-payload ratio which is better than 2 : 1, is able to handle masses of up to 10 kg at full dynamics, and is equipped with a control unit and power supply. The modular arm can be configurated according to the specific application and thus perfectly adjusted to various tasks.
Pour en savoir plus…
|
|
|
01.04.2010
Heavy Duty Gripping Systems for Wind Power Stations
Industrial robots can now lift weights of a ton or more. For building wind power stations, such "powerhouses" open new potentials in productivity. For assuring a reliable grip of bearings, hubs and other heavy components, SCHUNK developed a heavy load gripper which achieves a stroke of 100 millimeters per finger a gripping force of 23,000 Newton.
Pour en savoir plus…
|
|
|
31.03.2010
Further gripper sizes for dirty environments
SCHUNK is extending its series of sealed grippers, the 2-Finger-Parallel Gripper DPG-plus is available in sizes 240 and 300 now. The actuation via an oval piston and the multi-tooth guidance provide a powerful, precise, and fail-safe handling of this gripper. Therefore a high machine availability, and consequently, a high profitable efficiency of manufacturing and assembly is assured.
Pour en savoir plus…
|
|
|
15.03.2010
Facilitating the Design of Modules
SCHUNK has improved its user-friendly modular system. With two software solutions "Toolbox Rotation" and "Toolbox Translation" every GEMOTEC system from the rotary and linear modules to the gantry modules can be designed. Therefore the high efficiency of individual components can be completely exploited and avoids an expensive over-sizing.
Pour en savoir plus…
|
|
|
01.03.2010
Third SCHUNK Expert Days Service Robotics
World-wide network of experts advances service robotics
On February 24 and 25, 2010, professionals from all over the world met at the third Expert Days on Service Robotics at SCHUNK in Lauffen, Germany, the technology leader in gripping and workholding. This world-wide symposium is considered to be the leading communication platform for applied service robotics. This is due to top-class attendees, which SCHUNK invites every year for this event, and the high dynamics involved by the topic itself. From a small group of thoughtleaders in robotics, an interdisciplinary global network developed, which is preparing the future for robots as a flexible aid in industrial and domestic environments .
Pour en savoir plus…
|
|
|
09.02.2010
All-in-One Palettiergreifsystem
Das standardisierte Palettiergreifsystem LEG des Lauffener Automationsspezialisten SCHUNK ist ein echter Alleskönner: Flexibel handhabt es im Wechsel Paletten, Zwischenlagen und verschiedene Produkte. Das Herzstück des Multifunktionsgreifers ist der Servo-Parallelgreifer LEG von SCHUNK.
Pour en savoir plus…
|
|
|
25.01.2010
Change the cycle type as you like
SCHUNK has enlarged its GEMOTEC modular system for modular assembly technology by a new pneumatically driven ring indexing table type RST-P, which can cycle either to the left or to the right or alternate without requiring any modifications.
Pour en savoir plus…
|
|
|
13.01.2010
New gripper sizes of the compact class
SCHUNK has expanded its compact class, the 2-Finger-Parallel Gripper type JGP and the 3-Finger-Centric Gripper type JGZ with the sizes 200, 240, and 300 now. All the modules are equipped with a powerful pneumatic oval or round piston drive and together with the compact dimensions, an excellent power density is achieved.
Pour en savoir plus…
|
|
|
07.01.2010
SCHUNK Expert Days - Service Robotics 2010
Expert forum for the future of service robotics
The first two Expert Days in 2008 and 2009 were a great success for all the participants. Now SCHUNK, the specialist in toolholding, workholding and automation in Lauffen, Germany, has organized the third Expert Days for service robotics on February 24 and 25, 2010. Experts from all over the world will assemble at this summit. In numerous lectures, which are held in English, the participiants will recieve information on present research projects, trends, and chances for service robotics.
Pour en savoir plus…
|
|
|
Communiqués de presse - Modules de Préhension - 2013
Communiqués de presse - Modules de Préhension - Archives 2012
Communiqués de presse - Modules de Préhension - Archives 2011
Communiqués de presse - Modules de Préhension - Archives 2010
Communiqués de presse - Modules de Préhension - Archives 2009
Communiqués de presse - Modules de Préhension - Archives 2008
Communiqués de presse - Modules de Préhension - Archives 2007
Communiqués de presse - Modules de Préhension - Archives 2006
Communiqués de presse - Modules de Préhension - Archives 2005
Communiqués de presse - Modules de Préhension - Archives 2004
Communiqués de presse - Modules de Préhension - Archives 2003
|
|
|