|
|
Communiqués de presse - Technique de serrage - Archives 2011
|
| |
|
21.12.2011
New catalog for Stationary Workholding
SCHUNK is the only manufacturer that offers a vast, standardized modular system for highly efficient workpiece clamping. The competence leader for clamping technology and gripping systems bundles its complete program on stationary workholding in a new catalog. For the first time, the VERO-S NSE mini - the world’s flattest pneumatic quick-change pallet module, the VERO-S NSL turn - a highly efficient clamping station for milling machining centers, the powerful VERO-S NSR robot coupling, and KONTEC KSX - a powerhouse for simultaneous 5-axis machining, are all included in one catalog. The Stationary Workholding catalog is now available, and can be ordered free of charge at www.schunk.com.
Pour en savoir plus…
|
|
|
20.10.2011
TRIBOS Clamping Device:
Compact, cost-efficient, quiet
The automatic TRIBOS SVP-4 clamping device from SCHUNK, the competence leader for clamping technology and gripping systems, is much more compact and lighter than its predecessor. Moreover, an innovative pump ensures that the device is especially quiet while working. On option, it can be operated with 220 V AC from the socket, or if required, operated mobil with rechargeable batteries. An intuitive control concept simplifies the clamping operation: the required clamping pressure for tool change can be continuously adjusted via a controller.
Pour en savoir plus…
|
|
|
20.10.2011
Status display for magnetic chucks
Operators will now be able to see at a glance whether the MAGNOS magnetic chucks from SCHUNK are activated or not. For this purpose, all the new square pole chucks from the competence leader for clamping technology and gripping systems are equipped with a permanent display which informs the operator on the clamping status of the magnetic chuck.
Pour en savoir plus…
|
|
|
20.10.2011
Laser welding at the limit
With the PSM 400 laser welding machine from SCHUNK Lasertechnik even demanding materials can be welded crack free and cost effectively. The machines are so flexible that both small and large components can be precisely machined. High-performance Nd:YAG lasers with pulse durations of up to 200 ms ensure convincing welding results, even in case of materials which are difficult to weld.
Pour en savoir plus…
|
|
|
20.10.2011
The most flat pneumatic Quick-Change Pallet Module in the world
SCHUNK, the competence leader for clamping technology and gripping
systems continues to enlarge its program of VERO-S Quick-Change Pallet System they will present at the EMO 2011 show. With a height of 20 mm, the VERO-S NSE mini module from SCHUNK is the most flat pneumatic Quick-Change Pallet Module in the world. This provides ideal conditions for retrofitting existing machines, making full use of the engine room, and allows direct clamping of small workpieces.
Pour en savoir plus…
|
|
|
20.10.2011
SCHUNK GmbH & Co. KG - A Short Profile
"To offer more than the customer expects", this was the motto of Friedrich Schunk, when he opened his machine shop in a garage in Lauffen, Germany, right after the troubles of World War II. Today, SCHUNK is a German innovative family-owned company and a global player all in one.
Pour en savoir plus…
|
|
|
17.10.2011
New Catalog for hydraulic expansion solutions
Customer-specific hydraulic expansion solutions are an effective possibility for minimizing set-up times and lowering costs at maximum precision. For presenting the large potential of this precision technology, SCHUNK, the competence leader for clamping technology and gripping systems has issued a catalog specifically for special solutions in the hydraulic expansion technology.
Pour en savoir plus…
|
|
|
12.10.2011
New edition of the best-seller ROTA-S plus
The manual ROTA-S plus lathe chuck from SCHUNK has been sold over 10000 times now. With version 2.0, the competence leader for clamping technology and gripping systems continues its success story with the highly efficient classic chuck: An optimized wedge bar drive system and an improved lubricant system ensure consistently high clamping forces from the new lathe chuck. Since higher speeds and cutting speeds are possible, users can apply more efficient cutting materials, which shorten the manufacturing time.
Pour en savoir plus…
|
|
|
12.10.2011
Status display for magnetic chucks
Operators will now be able to see at a glance whether the MAGNOS magnetic chucks from SCHUNK are activated or not. For this purpose, all the new square pole chucks from the competence leader for clamping technology and gripping systems are equipped with a permanent display which informs the operator on the clamping status of the magnetic chuck. The display is completely independent from the main energy supply, and users, who already work with the MAGNOS magnetic chucks, can order a retrofit set for existing magnets from the innovative family-owned company.
Pour en savoir plus…
|
|
|
12.10.2011
TRIBOS Clamping Device:
Compact, cost-efficient, quiet
The TRIBOS polygonal clamping technology from SCHUNK is one of the world’s most comprehensive programs for high-precision tool clamping. From micro to volume cutting, the patented clamping system of the competence leader for clamping technology and gripping systems scores with permanently high true-running accuracy, convincing vibration damping, and the possibility to pre-adjust the length to exactly where you want it. The innovative family-owned company showcases a completely modified universal clamping device at the EMO show now, which clamps all TRIBOS mountings quickly, precisely and energy-efficiently. The highlight: since the manufacturing costs were reduced, the new clamping device can be offered at a highly affordable price.
Pour en savoir plus…
|
|
|
11.10.2011
Producing more efficient
For a number of years, everybody was talking about the energy efficiency issue. Increasing energy costs, a growing environmental awareness, and the political guidance were all triggers for many companies to highlight the energy consumption of machines and components in their communication with the public. Efficiency is much more than simple energy efficiency now, especially when considering the
time- and cost aspects in regards to efficiency. When all these factors have been considered in a holistic way, the full potentials for modern machining and production become visible. The modern clamping devices and gripping systems make it clear how complex the possibilities are.
Pour en savoir plus…
|
|
|
28.09.2011
Lightweight design - Lathe chucks available in three versions
Shorter cycle times, lower energy consumption, less wear - weight-reduced lathe chucks offer an entire package of benefits. The key is knowing the best one to pick from the technogical and economic point of view? With the ROTA NCL lightweight lathe chuck, SCHUNK, the competence leader for clamping technology and gripping systems wants to find the answer on this question. The powerful lightweight is available in three versions: As a weight-optimized steel-, a light aluminum-, and in an ultra-light carbon version.
Pour en savoir plus…
|
|
|
28.09.2011
Electric Quick-Change Pallet Module
With the electric version of the VERO-S NSE mini quick-change pallet module, SCHUNK, the competence leader for clamping technology and gripping systems has now made an important contribution to the electrification of machine tools. Instead of being actuated by compressed air, the technology study of the electric module is actuated via a torque motor, and separate engine control is no longer required. A patented drive concept provides for pull-in forces of up to 1,000 N.
Pour en savoir plus…
|
|
|
08.08.2011
A new catalog "Toolholding Systems"
Just in time for the EMO show, SCHUNK, the competence leader for clamping technology and gripping systems, is issuing a new catalog on toolholding systems. Highlights include the powerful TENDO-E hydraulic expansion toolholder and the TRIBOS-Mini, the first precision toolholder for direct clamping of very small shank diameters used for micro cutting. The catalog will hold the complete total tooling program of the innovative family-owned company.
Pour en savoir plus…
|
|
|
03.08.2011
Light, low maintenance and multi-purpose
The ROTA NCL lightweight lathe chuck from SCHUNK, the competence leader for clamping technology and gripping systems, newly defines efficiency for turning operations. The ROTA NCL steel version weighs about 35% less compared to conventional power chucks of the same size. Therefore faster acceleration at a reduced energy consumption is possible. A new type of double cylinder guidance of the base jaws ensures that the forces are evenly distributed on the chuck body. With its large through-hole, the lathe chuck is almost maintenance-free, completely sealed and permanently lubricated, making it perfectly suitable for applications in modern machining centers.
Pour en savoir plus…
|
|
|
03.08.2011
More precise in deepest angles
SCHUNK, the competence leader for clamping technology and gripping systems, has continued to enlarge its program of slim hydraulic extensions to be presented at the 2011 EMO show. With a shank diameter of 6 mm, the TENDO SVL tools can be directly clamped without the use of intermediate sleeves, making them highly precise.
Pour en savoir plus…
|
|
|
03.08.2011
The most flat pneumatic Quick-Change Pallet Module in the world
SCHUNK, the competence leader for clamping technology and gripping
systems continues to enlarge its program of VERO-S Quick-Change Pallet System they will present at the EMO 2011 show. With a height of 20 mm, the VERO-S NSE mini module from SCHUNK is the most flat pneumatic Quick-Change Pallet Module in the world. This provides ideal conditions for retrofitting existing machines, making full use of the engine room, and allows direct clamping of small workpieces.
Pour en savoir plus…
|
|
|
20.07.2011
Zahlreiche Jugendliche nutzten Schnuppertag bei SCHUNK
Null Bock war gestern. Heute halten Jugendliche offensichtlich ihre Nase in den Wind, wenn es darum geht, berufliche Zukunftschancen auszuloten. Entsprechend groß war der Andrang beim Schnuppertag, den der Kompetenzführer für Spanntechnik und Greifsysteme SCHUNK am vergangenen Samstag in seinem Ausbildungszentrum in Lauffen veranstaltet hat. Verglichen mit dem Vorjahr hat sich die Zahl der Besucher in diesem Jahr glatt verdoppelt.
Pour en savoir plus…
|
|
|
20.06.2011
Powerhouse for 5-axis machining
The KONTEC KSX NC vise from SCHUNK is a powerful clamping system for simultaneous 5-axis machining. The compact, and easily accessible clamping system from the competence leader for clamping technology and gripping systems disposes of tool-free adjustable clamping forces between 4 and 40 kN, which are measured directly at the workpiece.
Pour en savoir plus…
|
|
|
09.03.2011
Flexible lathe chuck for a high efficiency during turning
The 3-jaw power chuck type ROTA NCD from SCHUNK, the competence leader in clamping technology and gripping systems is an all-rounder for high-precision workpiece clamping on lathes. It is particularly well suited for users who machine several workpieces on one machine and can reduce set-up times and costs with the high-performance lathe chuck.
Pour en savoir plus…
|
|
|
09.03.2011
ROTA NCS Power Chucks: High precision and low maintenance
"The lathe chuck technology of the future." - this is what the sealed 3- or 6-jaw power chucks type ROTA NCS from SCHUNK are called by those who use them. The innovative lathe chuck from the competence leader in clamping technology and gripping systems combines high clamping forces, maximum precision and minimum effort. In view of the continuously increasing quality requirements in modern metal cutting, the benefits of the ROTA NCS ensure a maximum investment safety.
Pour en savoir plus…
|
|
|
16.02.2011
The Lathe Chuck Catalog has been modified
The SCHUNK lathe chuck catalog is now available. The catalog provides 660 pages information on the complete workholding program of SCHUNK, the competence leader in clamping technology and gripping systems. From lathe chucks to steady rests, jaw boxes up to accessories, everything is listed.
Pour en savoir plus…
|
|
|
Communiqués de presse - Technique de serrage - 2013
Communiqués de presse - Technique de serrage - Archives 2012
Communiqués de presse - Technique de serrage - Archives 2011
Communiqués de presse - Technique de serrage - Archives 2010
Communiqués de presse - Technique de serrage - Archives 2009
Communiqués de presse - Technique de serrage - Archives 2008
Communiqués de presse - Technique de serrage - Archives 2007
Communiqués de presse - Technique de serrage - Archives 2006
Communiqués de presse - Technique de serrage - Archives 2005
Communiqués de presse - Technique de serrage - Archives 2004
Communiqués de presse - Technique de serrage - Archives 2003
|
|
|