|
|
In Focus - Archive December 2010
|
| |
| |
|
|
12.2010
Clamping large turned parts safely
Launched from the energy technology, machining of large parts on lathes has become more important in the past few years. This causes a lot of pressure which has to be absorbed by the clamping device. This factor makes it all the more surprising that many users still use traditional clamping solutions, which are costly to set-up, clean and maintain. Modern clamping devices do more than assuring safe clamping, they increase precision of the workpiece, reduce set-up times, and minimize maintenance efforts. This also applies for chucks and jaw boxes.
more...
|
| |
|
|
10.2010
Grippers with additional benefits
The figures speak for themselves: SCHUNK, the leading expert for clamping technology and gripping systems has sold thousands of sensors for handling applications. While the status of the actuator has been monitored in the past, modern sensors transform the grippers into intelligent helpers, which can measure, inspect, sort and accelerate the whole process simultaneously. The question on their efficiency potential is answered with an overview of the current sensor systems for handling applications.
more...
|
| |
|
|
09.2010
Gripping Technology for Industrial Robots
Industrial robots work quickly, reliably and never stop. The achieved output and quality significantly depends on the individual periphery, particlularly of the gripping sytems. In the hunt of the optimum gripper, engineers and users have to consider a large variety of influencing factors. In addition to efficiency and process-reliability, sustainability of the gripping systems playes an increasing role.
more...
|
| |
|
|
08.2010
Efficient toolholders for automated tool grinding
For tool grinding the toolholder plays an essential role because microns will decide the quality of the manufactured tool edges. In view of small batch sizes and various tools, a multi-purpose toolholder is needed. The holder would have to be precise for exact cutting edge geometries and surfaces, slim to avoid interference between the grinding wheel, powerful for very short clamping depths, and have a high material removal rate as well. Flexibility is also required for covering many different shaft diameters. All of these requirements are persuading companies to use automated grinding machines in order to reduce their current costs.
more...
|
| |
|
|
07.2010
Pick & Place Solutions in Comparison
In order to assemble components fast and precisely, operators can choose between many different Pick & Place solutions. The performance features of the systems vary from each other. To find the best solution, the advantages and disadvantages of each system should be compared.
more...
|
| |
|
|
06.2010
Energy efficient gripping
In the best of case scenario, energy-efficient automation modules should reduce energy consumption of the handling system and increase cycle times and output. It helps conserve the environment and saves money if you focus both measures.
more...
|
| |
|
|
05.2010
Factor of Success Engineering -
With virtual simulations to the optimum clamping solution
How does a component deform during the clamping process and machining? Which clamping solution assures that the workpiece has the exact dimensions? How can an existing clamping device be ideally used? Virtual simulations are giving valuable answers to these and simular questions. By means of the Finite Elements Method (FEM) deformations and component payloads can be calculated, which allows a comparison of the individual clamping options and how to optimize them. In turn, process and investment reliability are increased, development times shorten, the selection of the suitable clamping device is easier and costs are lowered.
more...
|
| |
|
|
04.2010
Magnetic Clamping Technology - efficient at a variety of tasks
Magnetism is one of the most fascinating and influential force of our universe. Engineers and technicians use this same force in order to clamp workpieces, or to reliably lift components. Magnetic clamping technology is well-established in various areas, such as grinding, milling, turning, mobile lifting units in production, and for huge crane constructions. Most engineers now know that magnetic clamping solutions reduce set-up times by about 80 percent, that workpieces are clamped without any deformation, and even coils can be reliably transported.
more...
|
| |
|
|
03.2010
EU-funded project pushes on the service robots
Experts predict an increase in the pursuit of service robotics. This is no surprise: Modern robot applications offer an enormous potential to the economy and society. Pilot applications already show how robots might become more and more the intelligent helpers of humans. In addition to universities and other research institutes, industrial enterprises should focus on development in this sector, and make it a reality. Therefore the European Union has decided to subsidize the transfer of knowledge between research institutes and industry financially support this pursuit as well.
more...
|
| |
|
|
02.2010
Flexible packing and palletizing
Adaptive handling systems provide dynamics and profitability if comprehensive ranges and frequent changes in assortment are given.
Every week a new product generation replaces the previous one. These products, which provide new impulses in trade, are a real challenge for the packing process. Faster, process reliable, and flexible automated solutions are in constant demand. They help to keep the handling costs under control, even at an increasing product variety.
more...
|
| |
|
|
01.2010
How operators "play it safe" during turning operation
If a workpiece loosens from the chuck on a lathe, it can be dangerous to those working in the manufacturing hall. Because of this, the Employer’s Liability Insurance Associations, Standards and Safety Commitees, do everything in their power, to avoid accidents.
more...
|
| |
|
| |
 |
 |
 |
| |
In Focus - 2013
In Focus - Archive 2012
In Focus - Archive 2011
In Focus - Archive 2010
In Focus - Archive 2009
In Focus - Archive 2008
In Focus - Archive 2007
|