|
|
 |
|
|
In Focus - Archives Décembre 2011
|
| |
| |
|
|
12.2011
Clamping solutions for automated mass production
Efficient manufacturing means automated manufacturing. This particularly applies if large series are machined. This is when the clamping vises, which are the direct interface to the workpiece, playing an important role. In only a few seconds, they have to mount the components, safely and precisely align them, clamp them with-out deformation, and after machining they have to be reliably released. In view of the several million clamping cycles, which have to be carried out by many clamping vises being exposed to chips and coolant, process reliability is one of the decisive factors of success.
Pour en savoir plus…
|
| |
|
|
11.2011
Modularity the factor of success
When designing gripping systems for handling and assembly applications, standardized modular systems will play an increasingly important role in the future. They reduce the necessary time for project planning and commissioning, and lower the investment costs. Due to the standardization, they offer optimum preconditions for stable processes. Since modular designed units can be flexibly modified and enlarged, they can be re-configurated for any changes that come up in the future.
Pour en savoir plus…
|
| |
|
|
10.2011
Producing more efficient
For a number of years, everybody was talking about the energy efficiency issue. Increasing energy costs, a growing environmental awareness, and the political guidance were all triggers for many companies to highlight the energy consumption of machines and components in their communication with the public. Efficiency is much more than simple energy efficiency now, especially when considering the
time- and cost aspects in regards to efficiency. When all these factors have been considered in a holistic way, the full potentials for modern machining and production become visible. The modern clamping devices and gripping systems make it clear how complex the possibilities are.
Pour en savoir plus…
|
| |
|
|
09.2011
Welding demanding materials crack- and pore-free
Laser welding technology is second-to-none, regardless of whether you are dealing with gears and injection molds or delicate and challenging welding works. When conventional cw lasers and many Nd:YAG-lasers reach their limits, modern process strategies can help to machine demanding welding metallurgies, different types of materials, or micro components process reliably and efficiently. Laser welding is particularly used if components have to be joined at a high welding speed, because slim welding seams, and a low thermal distortion are required. Compared with other welding techniques, the energy during laser welding fully penetrates into the material.
Pour en savoir plus…
|
| |
|
|
08.2011
More than a "Stopgap": Intermediate sleeves ensure safe clamping and precision
They appear to be unimposing - but they are located at a decisive interface in the chain of the metal cutting process. Between toolholder and workpiece, the intermediate sleeves influence reliability and precision of the clamping operation. The thin-walled, mostly slotted precision sleeves cover the difference between the clamping diameter of the toolholder, and the workpiece which has to be clamped. Functioning like reduction inserts, they multiply the fields of application of the toolholders or arbors, compensate tolerances, and ensure safe and gentle clamping of gear wheels. The newest sleeve design can do even more. Intermediate sleeves with nozzle effect extend the tool service life and increase the volume machining.
Pour en savoir plus…
|
| |
|
|
07.2011
Changing, machining, compensating -
current trends in robot accessories
In dealing with industrial robot efficiency cycle rate and process reliabilty largely depend on their front ends, the grippers and other tools, but also from the effectors’ interfaces to the robot arm. Robot accessories have a great influence on the robot’s performance, flexibility and fields of application. Latest developments of quick-change systems, driven tools, compensation units, and power sensors show that the potentials of modern accessory components are enormous. Experts assume that their importance for handling, assembly and manufacturing will continuously increase.
Pour en savoir plus…
|
| |
|
|
06.2011
Deformation-free clamping:
From the plastic chuck jaw to the hybrid chuck
In case of rings, housings and other workpieces which are highly deformable dur-ing processing, conventional 3-jaw chucks quickly reach their limits. If the clamping forces are too low, there is no secure hold. If they are increased, workpieces de-form, and precision is reduced. A comparison shows the alternatives, the differ-ence between them, and how users can achieve an optimum result.
Pour en savoir plus…
|
| |
|
|
05.2011
Service robotics is the future key market
Insiders are convinced that golden times lie ahead for service robotics. Around the world companies and institutes have recognized the potential of robots as helpers for humans, and are working on everyday solutions. All different kinds of businesses are interested in service robotics, from large companies, to innovative startups, and also conventional manufacturers of industrial robots, electronic and automation components.
Pour en savoir plus…
|
| |
|
|
04.2011
Having set-up times under control
You cannot earn money with a turned off machine. However, in many companies the workpieces are still set-up in a complicated and time-consuming way on a grooved table while the plant is turned off. But solutions exist, which optimize the machine tool load. Modern quick-change pallet systems demonstrably accelerate the machining process, and at the same time, ramp up the precision and process reliability score. This leads to a reduction of set-up costs of up to 90%.
Pour en savoir plus…
|
| |
|
|
03.2011
Toolholders for micro cutting
Clamping tools used for micro cutting have their own rules. The subtle tools, the high spindle speeds, and the extreme precision requirements are a challenge for every tool manufacturer and user. Those who want to achieve continuously precise results, need mountings with a high run-out accuracy and balancing grade. Moreover, they should be as slim as possible and resistant to dirt. Furthermore, they have to assure that even small tools can be precisely adjusted and exchanged.
Pour en savoir plus…
|
| |
|
|
02.2011
Leight-weight design increases efficiency of Gripping Systems
Light-weight modules are now playing an increasing role in the area of gripping systems. Integrated into the system, they are saving energy at the same efficiency, or achieve a considerably higher efficiency at the indentical energy consumption. In both cases, the efficiency of the whole system is increasing. This is why the lightweights are so interesting for plant manufacturers, system integrators, and users. Since light-weight solutions had the reputation of being overly expensive in the past, recent developments now show that efficiency and cost control can go hand-in-hand. Modern designs, materials and techniques are paving the way to lighter solutions, which are rigid and robust, too. This also offer many more advantages.
Pour en savoir plus…
|
| |
|
| |
 |
 |
 |
| |
In Focus - 2013
In Focus - Archives 2012
In Focus - Archives 2011
In Focus - Archives 2010
In Focus - Archives 2009
In Focus - Archives 2008
In Focus - Archives 2007
|
|