|
|
 |
|
|
In Focus - Archive February 2009
|
| |
|
|
|
02.02.2009 -
With 87,000 employees and sales of around €14 billion in 2007, the foundry sector is one of German industry's smaller branches. Its economic significance is large, however, because hardly any other industry can function without cast parts of steel, aluminum or copper and copper alloys.
Germany is the largest casting manufacturer in Europe, and ranks number 6 in the world. The 265 German iron and steel foundries achieved a production volume of 4.8 million tons in 2007, while its 342 companies in the non-ferrous casting sector had a production level of 1.1 million tons. The vehicle and mechanical engineering sector is the principal customer for cast products. It has a 79% share of total casting production.
|
|
High degree of automation
|
 |
The sprue and runners are stripped after the part is placed on a die.
|
|
 |
In the past few years, many foundries have systematically expanded their added value chains and now provide the service of mechanically processing cast parts to their customers, for example. Driven by competitive pressure and exacting demands on quality and flexibility, many foundries rely on automation as much as possible: using robots in production is practically a matter of course.
Almost no other industrial sector places such exacting demands on the resistance of the automation components it uses. High temperatures, abrasive dust from sand cores and dies, steam, and hot, aggressive gases eat away at guides, clog seals, and have an adverse affect on lubricants.
Grippers are especially affected because they are on the front line and therefore exposed to the highest strain. They grip hot or still-glowing parts immediately after casting, are exposed to metal scrap, release agents, and core sand when dies are blown out, and have to withstand water and hot steam when pieces are cooling.
But there are also extreme conditions in the outlying areas of the foundry sector, where the temperatures are more moderate. Workpieces there are processed by chamfering, sawing or grinding for example, and the automation components used are also exposed to adverse conditions.
|
|
Exacting demands require special components
|
|
SCHUNK provides numerous components for companies in the foundry sector. With their rugged design, they are able to withstand the highest amount of strain and can also be prepared for especially tough conditions and high temperatures by taking advantage of numerous options.
|
|
Corrosion and dust protection
|
 |
PGN plus gripper
|
|
 |
SCHUNK provides optional corrosion protection to increase the corrosion and abrasion resistance of a gripper or swivel unit, for example. Base jaw guides and the wedge and piston kinematics can be equipped with an extremely hard coating. This increases resistance to abrasive dust, reduces internal friction and the amount of lubrication required and extends the service life of the entire gripper.
To reduce the amount of dust that penetrates the gripper, many grippers have optional dust protection which shields the guides with an additional cover.
Applying sealing air also prevents penetration by particles from the environment. This is done by applying compressed air to the inside of the gripper through its sealing air connection. This causes a slight air current to emerge from the gap between the guides and the housing, which prevents most of the smallest particles from penetrating.
Series PGN plus grippers, used for high temperature applications, are also available in a special foundry design. With options such as an expanded protective enclosure and the use of a special lubricant, SCHUNK has made sure that the grippers have high thermal resistance. Because less ceramic materials are used in the base jaws, the thermal conductivity from the gripper fingers to the grippers is reduced. That means that the foundry design can also be applied to forging and casting processes whose workpieces have extremely high temperatures.
|
|
Multi-tooth guide
|
 |
PZN plus gripper
|
|
 |
The multi-tooth guide developed and patented by SCHUNK also plays an important role in the foundry sector because it contributes to increasing the load capacity of grippers.
The multi-tooth guide permits forces and torques to be distributed among several guide surfaces instead of only one as in the case of the classical T-slot. That means that the guides have a higher load capacity and the "jamming effect" is reduced. It also introduces the option of using longer gripper fingers for the same gripper size without overloading the guides.
The base jaws are fit into the housing with an accuracy of 0.01 mm, which also minimizes guide play and wear. As a consequence, components that are equipped with a multi-tooth guide are characterized by especially high load capacity and service life – the best prerequisites for use in foundries.
SCHUNK's product range contains many grippers that are equipped with a multi-tooth guide. They include the pneumatic parallel grippers in the PGN plus series and their 3-finger counterparts in the PZN plus series, the PGB series with its end-to-end center bore, the DPG plus sealed gripper, the servo electrical EZN 64 3-finger centric gripper and the PZV 4-finger centric gripper.
|
|
Direct from the field: SCHUNK foundry applications
|
|
SCHUNK components are used everywhere in the foundry sector. The following examples provide a brief overview of SCHUNK components' broad application spectrum.
|
|
Handling red-hot cast-iron parts
|
 |
1: 2-finger long-stroke gripper PFH 30 in protective enclosure
2: Stainless steel finger
|
|
 |
In a foundry, the red-hot forged blanks received from a handling system are placed in a cooling tank. To protect the parallel gripper from the high temperature, it is equipped with stainless steel fingers to minimize thermal conductivity. Additional air cooling from the outside prevents the gripper unit from overheating. To prevent dirt from penetrating into the gripper unit, a special sealing air connection has been integrated. With this equipment, the handling system provides highly reliable performance with a minimum of maintenance costs.
|
|
Sand core handling at Grohe
|
 |
Safe, gentle grip with glass fiber molding jaws
|
|
 |
In its foundry in Hemer, Germany, fittings manufacturer Grohe uses preformed sand cores to manufacture brass blanks. The cores are produced using an injection molding process, which means that the finished products have pin marks and flash. Grohe uses robotics to remove them. The robots receive the sand cores, check them for core fracture at a sensor barrier, and then guide them past a stationary carbide cutter that removes pin marks and flash. To remove flash, the sand cores are pulled through a beaded curtain that removes all burrs with its metal chain.
All of the robots are equipped with the SCHUNK PGN plus 80 gripper in the dust protection design. Because the cores are very fragile and have to be gripped with perfectly accurate molding jaws at the exact points specified, Grohe uses glass fiber gripper fingers from the SCHUNK range that are manufactured using a special laserforming process. The grippers are equipped with the quick-change jaw system so that suitable gripper fingers can be fitted within a few seconds when changing over to a different product.
|
|
Foundry automation at Amann
|
 |
Caption: A double gripper can handle two parts per cycle
|
|
 |
Amann Druckguss GmbH from Massenbachhausen, Germany produces transmission casings and mounts, clutch bells and parts for radiator applications for the automotive industry.
Amann uses a total of 15 foundry-design robots for loading and unloading die casting machines and the connected dies. Six PZN plus 100 series centric grippers are used for gripping round parts. Amann also uses numerous parallel grippers in the PGN plus 125 premium series, sometimes combining them into double grippers so that larger parts can be gripped at several points at the same time. A PGN plus 300 that can deal with workpiece weights of up to 30 kg is also used for handling entire transmission casings.
All of the grippers are equipped with optional dust protection equipment. They are also equipped with Viton seals that can survive temperatures of up to 130° without damage and can therefore be used in extremely hot environments. Sealed air is also applied to some of the gripper modules to prevent the penetration of dust and slag, increasing the service life of the grippers.
|
|
| |
|
| |
 |
 |
 |
| |
|
|
11.2009
Straightaway micron-precise
In addition to a high repeat accuracy, in modern machine tools, positioning-, measuring- and handling the accuracy of the axial movement is now playing an important role. In this way, precise parts for the production or electronic industry, can be designed with a micron-precise guidance along the complete axis.
more...
|
| |
|
|
10.2009
How Machines Can Learn To See
More and more industries tap the full potential of machine vision systems. Whether in the supermarket, on the highway, at the airport, or in the factory; pictures are being taken by a camera system and are evaluated with a computer, in order to make a fully-automatic, quick and safe decision.
more...
|
| |
|
|
09.2009
Hydraulic expansion technology for workpiece clamping
Hydraulic expansion toolholders for tool clamping (milling cutter, drills, taps and reamers) are known on the market for a long time and are appreciated for their technical advantages. They combine powerful, centric clamping with a high internal dampening. The result is an excellent surface at high machining speeds.
more...
|
| |
|
|
08.2009
Gripping - checking - measuring - preventing from damage
Intelligent sensors transform actuators to sensitive helpers in automation
Sensors used in automation are essential organs of machines and plants. While gripping modules and other actuators performed pre-defined tasks in the past, today, they are intelligent and flexible helpers in the manufacturing process due to the use of intelligent sensors. They provide the plant with important information on the process, products or components as well as plant functions. This increases flexibility, shortens manufacturing time, ensures product quality, avoids plant failures, and prevents the automation systems from damage.
more...
|
| |
|
|
07.2009
The trend towards precision toolholders
For many years, collet chucks have been popular because of their low pricing and have been the established toolholders for many machining applications. Unfortunately, the same scenario happens in many companies: Because of worry over loose tools, many machine operators are tightening the coolant tube nut of the collet mountings with oversized extensions.
more...
|
| |
|
|
06.2009
Always up-to-date with the standards - The new machinery directive in the EC
The safety of products and systems traditionally tops the priority list at SCHUNK. Since we want to partner with our customers, we are exclusively offering top-of-the-line products in quality and safety.
more...
|
| |
|
|
05.2009
Highly economical due to performance in toolholding and workholding
5-axis machines offer an enormous potential for efficiency in modern production. With sturdy machine kinematics, high axis accelerations, short chip-to-chip times, fast tool magazines and finely tuned controllers, you have all kinds of production power in a very small space.
more...
|
| |
|
|
04.2009
Microvalve Technology
- Small component handling and assembly
Anyone who wants to handle or assemble small, light parts can really get a move on with electromagnetic microvalves. These energy-efficient valves are screwed directly onto the pneumatic actuator and thus eliminate the need for long wires. They make the tempo significantly faster and thus save compressed air, complicated wiring, and a lot of assembly time.
more...
|
| |
|
|
03.2009
Reliable precision for the most well-hidden corners
Regardless of their design sophistication, it is sometimes impossible to avoid cre-ating hard-to-reach points on workpieces. All of these cases require slim toolholder systems with minimized interference contours. They have to penetrate into the most well-hidden corners, transmit sufficient torque and guarantee high precision at the same time.
more...
|
| |
|
|
02.2009
The foundry sector: a red-hot key industry
With 87,000 employees and sales of around €14 billion in 2007, the foundry sector is one of German industry's smaller branches. Its economic significance is large.
more...
|
| |
|
| |
 |
 |
 |
| |
In Focus - 2013
In Focus - Archive 2012
In Focus - Archive 2011
In Focus - Archive 2010
In Focus - Archive 2009
In Focus - Archive 2008
In Focus - Archive 2007
|
|